Einleitung
Customised automation and robotics solutions for the automotive industryItalian engineering skills meet Line XMS
Vensys: Automation made easy
- Requirements analysis and troubleshooting
- Machine design and testing
- Commissioning and maintenance
- Software development
Two customised solutions, one flexible basis
When he discovered Line XMS from item, it was love at first sight. He was particularly impressed by its lightness, stability and attractive appearance, among other characteristics.
Customised robotic soldering station
A specific solution for a specific problemTip soldering robot at Vensys
It uses a machine cabin based on Line XMS from item. A four-axis SCARA robot is installed inside the machine cabin.
The challengeAutomating the process of connecting plugs and printed circuit boards
“One of our customers initially tried to solve the problem using a standard solution from its supply chain, but without success,” reveals Zecchin.
A customised solution was therefore needed for the problem – and the idea for the tip soldering robot was born.
The soldering station in practiceHow the Vensys solution works
Soldering robots – offering benefits you can rely on
Further benefits:
- Errors reduced to a minimum
- Greater speed
- Optimised use of solder
Blinkermontage- und Prüfmaschine
Machine for assembling and testing electronic flasher unitsAssemble, test, label
At the heart of the solution is a rotary table with four positions. This table takes the constituent parts of a flasher unit to the processing stations.
A complex challengeA successful outcome within a year
All in all, it took around a year to design, build, test and deliver the application. “The end user is now enjoying all the benefits,” reports Zecchin with satisfaction.
Flasher unit gaining momentumHow the assembly and test machine works
Second station
An image sensor records the light output. Flash frequency is governed by legal requirements, so this is tested, too. If the parameters fail to comply with the legal requirements, the flasher unit is reported as faulty. It is then returned to the loading station, where it is rejected by the machine operator.
Third and fourth stations
On the next page, a video shows the complete process in action (video length: 1:22).
item Baureihe XMS
Why XMS from item was the perfect solution.“Line XMS from item gave us everything we were looking for.” – Mauro Zecchin.
Vensys particularly appreciates the large range of accessories for Line XMS, which ensures projects can be tailored to highly specific requirements and delivered in full. This brings a great deal of flexibility to machine cabin design. Fast, precise assembly with a minimum of effort is another key benefit.
All-round satisfaction“The products from item are extremely robust and well thought out.”
Vensys is keen to embark on further projects with item in the future.
Further information:
Vensys
Line XMS from item
Epson T3-B401S